Post Go back to editing

ADXRS649 Voltage range for VRatio while VS=5V?

Category: Datasheet/Specs
Product Number: ADXRS49

ADXRS649 Datasheet specifies all data at VS = AVCC = VDD = VRATIO = 5 V. In my system, a 0-3.3 V output is beneficial. I am currently using the eval board with external voltage dividers for the gyro and the temp output to scale them down, which works ok. I wonder if I can omit the external dividers and directly supply VRATIO with 3.3 V? Thus, VS = AVCC = VDD = 5 V while VRATIO = 3.3 V. Is this a supported mode of operation? 

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.