Post Go back to editing

AD5941 is Noisy in Several Freq

Category: Hardware
Product Number: AD5941

Hi, I am getting noisy readings from the AD5941 (custom PCB) at several random frequencies, this noise occurs at different frequencies for each board

Could this be related to the unused analog pins (AFE1-4, AIN0/3/4, SE0, DE0, RE0) that I’ve left floating?



Kind Regards,

Specia

  • No. Floating pins don't affect the measurement unless you use those pins for acquisition in your code.

  • I am using the following switch matrix configuration:

    Mux Settings: SWD_CE0 | SWD_AIN1, SWP_PL, SWN_NL, SWT_TRTIA | SWT_AIN2

    FYI the noise increases also over time, even without load on the probes

    Do you have any recommendations on where to look for the root cause of this noise issue?

    Is that possible, that the random noise coming from the moisture sensitivity?

    pre-heating before reflow the AD chip makes this issue solved (even using a previously used chip that was known to have issues). Seems like parasitic leakage (internally) that is caused by the moisture sensitivity? Since this issue always occurred at random frequencies (not at certain freq).

    Kind Regards,

    Specia

  • Could be due to moisture sensitivity, since it works fine after pre-heating.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.