Hi there,
We are attempting to interface with the ADXL367 accelerometer: Our application requires the accelerometer to be in Measurement Mode, with a sample-rate of 100Hz and measurement range of +-8g. At this stage, no activity or inactivity detection is required. The internal FIFO is also not used.
We are currently able to put the accelerometer into Wake-Up Mode (with sample rate of 12.5Hz). However, when attempting to put the device into Measurement Mode the ERR_USER_REGS bit is set in the STATUS register.
The following is our initialisation process. I have also included a screenshot of our hardware configuration for reference.


The device DEVID_AD, DEVID_MST, PART_ID, REV_ID, and SERIAL_NUMBER all read as their reset value.
Are you able to provide the initialisation process required for the device to enter measurement mode?
Happy to provide further information if needed.
Thanks,
Lachlan