Hello,
We are using the ADXL357 device as a vibration sensor in our custom board. The device has been configured as per the attached configuration register settings. However, we are not observing any activity interrupts on the INT1 pin.We have set the activity threshold to 5000 (≈ 0.0975 g, calculated as 5000 × 19.5 µg/LSB).
static int adxl357_simple(char* args, char* response){
UNUSED(args); UNUSED(response);
char str[64];
UART_PutString("Configuring ADXL357...\r\n");
// === Step 1: Basic Configuration ===
uint8_t i2c_speed = 0x01; // Setting I2C Speed to 400KHz
I2CWriteBytes(0x1D, 0x2C, 1, &i2c_speed);
uint8_t odr_value = 0x0A; // Output Data Rate set to 500Hz
I2CWriteBytes(0x1D, 0x28, 1, &odr_value);
uint8_t act_en = 0x01; // Activity enable register
I2CWriteBytes(0x1D, 0x24, 1, &act_en);
uint8_t act_count = 0x01; // Activity count
I2CWriteBytes(0x1D, 0x27, 1, &act_count);
uint8_t intr_ftn = 0x18; // Interrupt function setting
I2CWriteBytes(0x1D, 0x2A, 1, &intr_ftn);
uint8_t act_th_h = 0x13; // Threshold Register High
I2CWriteBytes(0x1D, 0x25, 1, &act_th_h);
uint8_t act_th_l = 0x88; // Threshold Register Low
I2CWriteBytes(0x1D, 0x26, 1, &act_th_l);
uint8_t x_offset_h = 0xFF; // X-axis offset High (-85 value in 2's compliment)
I2CWriteBytes(0x1D, 0x1E, 1, &x_offset_h);
uint8_t x_offset_l = 0xAB; // X-axis offset Low (-85 value in 2's compliment)
I2CWriteBytes(0x1D, 0x1F, 1, &x_offset_l);
uint8_t y_offset_h = 0xFF; // Y-axis offset High (-125 value in 2's compliment)
I2CWriteBytes(0x1D, 0x20, 1, &y_offset_h);
uint8_t y_offset_l = 0x83; // Y-axis offset Low (-125 value in 2's compliment)
I2CWriteBytes(0x1D, 0x21, 1, &y_offset_l);
uint8_t z_offset_h = 0x00; // Z-axis offset High (185 value in 2's compliment)
I2CWriteBytes(0x1D, 0x22, 1, &z_offset_h);
uint8_t z_offset_l = 0xB9; // Z-axis offset Low (185 value in 2's compliment)
I2CWriteBytes(0x1D, 0x23, 1, &z_offset_l);
uint8_t measurement_value = 0x00; // Measurement
I2CWriteBytes(0x1D, 0x2D, 1, &measurement_value);
UART_PutString("Registers configured.\r\n");
// === Step 2: Loop and read X/Y/Z every 2s ===
while (1)
{
uint8_t buf[9];
uint8_t intr_stat;
int32_t x, y, z;
float x_g, y_g, z_g;
// Burst read 9 bytes: XDATA3..ZDATA1
I2CReadBytes(0x1D, 0x08, 9, buf);
// X-axis
x = ((int32_t)buf[0] << 16) | ((int32_t)buf[1] << 8) | buf[2];
x >>= 4;
if (x & 0x80000) x |= 0xFFF00000;
// Y-axis
y = ((int32_t)buf[3] << 16) | ((int32_t)buf[4] << 8) | buf[5];
y >>= 4;
if (y & 0x80000) y |= 0xFFF00000;
// Z-axis
z = ((int32_t)buf[6] << 16) | ((int32_t)buf[7] << 8) | buf[8];
z >>= 4;
if (z & 0x80000) z |= 0xFFF00000;
x_g = convert_to_g(x, sensitivity);
y_g = convert_to_g(y, sensitivity);
z_g = convert_to_g(z, sensitivity);
char str[64];
sprintf(str, "X=%.3f g Y=%.3f g Z=%.3f g\r\n", x_g, y_g, z_g);
UART_PutString(str);
//sprintf(str, "X=%ld Y=%ld Z=%ld\r\n", x, y, z);
//UART_PutString(str);
//char str[64];
//sprintf(str, "Sensitivity =%.3f \r\n", sensitivity);
//UART_PutString(str);
UART_PutString("*****************************\r\n");
I2CReadBytes(0x1D, 0x04, 1, &intr_stat);
sprintf(str, "ADXL357 Interrupt Status = 0x%02X\r\n", intr_stat);
UART_PutString(str);
UART_PutString("-----------------------------\r\n"); // separator line
//CyDelay(1000); // wait 1 seconds
}
return 1;
}
As per the attached serial port log, the X-axis data crosses 0.1 g multiple times, but the INT1 pin does not show any interrupt.
For reference, we have also attached oscilloscope waveforms showing:
Yellow waveform – INT1 pin (configured for activity interrupt)
Green waveform – INT2 pin (configured for data-ready interrupt)

Request your guidance in resolving this issue.
Regards,
Prashant