Post Go back to editing

About the current consumption.

Thread Summary

The user asked if the IDD current listed in the ADXL343 datasheet (Tables 7 and 8) and the current consumed in Auto Sleep mode (typ. 23 μA) are the total current consumed by both Vs and VDD I/O. The support engineer confirmed that these values represent the total sensor consumption. The user, a DFAE, is gathering more details about the customer's IoT application and may have further questions.
AI Generated Content
Category: Hardware
Product Number: ADXL343

Hello team,

I would like to ask two questions about the ADXL343's current consumption.

①Regarding the IDD current listed in Table 7 and Table 8 on page 12 of the datasheet,
 should I understand this as the total current consumed by both Vs and VDD I/O?

②Similarly, is the current consumed in Auto Sleep mode (typ. 23 µA) also the total
 current consumed by both Vs and VDD I/O?

Best regards,
Tsuyoshi Tokumoto