Post Go back to editing

Problems converting negative acceleration data

Thread Summary

The user is experiencing unexpected -2.03 values on the x and y axes of an ADXL362 accelerometer in 16-bit 2g mode, despite expecting values close to 0. The final answer provides code snippets for data conversion, suggesting a potential issue with the sign handling or scaling factor. The z-axis shows a consistent offset of around 0.3, which may indicate a calibration or configuration issue.
AI Generated Content
Category: Hardware
Product Number: ADXL362

I'm using a ADXL362 in 16-bit mode in the 2g mode.

The function I'm using to read for the axis data registers,

void ADXL_ReadXYZ_16(uint16 *x, uint16* y, uint16*z)

{

    SPI_ReadRegister(0x0E, rawData, 6);

    *x = (uint16_t)((rawData[1] << 8) | rawData[0]);

    *y = (uint16_t)((rawData[3] << 8) | rawData[2]);

    *z = (uint16_t)((rawData[5] << 8) | rawData[4]);

}

Snippet for conversion of z-axis (the same procedure for the other 2 axes) 

AXDL362_ReadXYZ_16(&uint16_x, &uint16_y, &uint16_z);

/* Check sign */

if ((uint16_z & 0xF000) == 0xF000)

    {

       z = -1 * ((float)((uint16_z - 0xFB00) / 1000.0; // 0xFB00 removes extended sign bit & the sign bit at bit 11, scale factor 1000 from datasheet

    }

    else

    {

        z = (float)(uint16_z) / 1000.0;

    }

Typical reading with the sensor flat on the bench,

x : 0.01    y : 0.01    z : 1.35

With sensor tilted in + y direction

x : 0.01 or -2.04  y : 1.01    z : 0.3 

With sensor tilted in - y direction

x : 0.02  y :  -1.01    z : 0.35 

With sensor tilted in + x direction

x : 1.02   y : 0.01    z : 0.48

With sensor tilted in - x direction

x : 1.10   y : -2.03    z : 0.34

So there appears to be consistent offset in z of around 0.3 but I don't get why I'm getting those -2.03 values on the x & y axes when I am expecting close to 0.

Can anyone shed any light on this for me?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.