Post Go back to editing

ADIS16475 burst mode after normal operation for dozens of hours,data all be 0

Category: Software
Product Number: ADIS16475

Hello, my MCU is stm32f407. When using the burst mode of 16475 to read data, after 20 hours of normal reading(Not fixed, but no more than 3 days), the read data will be all 0, and this phenomenon can be stably reproduced.
My 16475 configuration is as follows:

1-FILT_CTRL=0x0006

2-DEC_RATE=0x0013 (ODR=2000/(1+19)=100hz)

My SPI configuration: 650k< 1M

My reading method:

After setting ODR to 100Hz, the MCU receives the external interrupt generated by the 16475 DR pin every 10ms. Read data in the interrupt:

Looking forward to your help!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.