Dear EngineerZone-forum,
in my thesis I need to precisely measure small rotation rates and hence decided to buy the ADIS16465-1 IMU, which can be operated using the EVAL-ADIS-FX3 evaluation board and the corresponding software. However I encounter two major problems while trying to operate the sensor.
1. The recorded rotation rates of the in-build gyroscope seem to be random. Without rotating the sensor at all, rotation rates of -600°/h are measured (see attached "Rotation Rates averaged over 100s)

I sadly do not understand how this is possible or if any calibration needs to be performed in order to fix this issue.
2. The noise level of the gyroscope is in the order of 0.2°/s, which is larger than any signal I want to record. Judging from the specified accuracy in the data sheet, such a high noise level should not be expected (see image "ADIS16465-1 Time Domain Plot)

Hence my question is , if anybody has encountered similar problems using the sensor and perhaps knows a fix or workaround to either reduce the noise level or to get reasonable rotation rates. I noticed that one can set the bias to shift the rotation rate, however if I choose the bias in such a way that I record my expected rates, I can not distinguish between my true signal and random noise/rotation rates recorded by the sensor. Therefore a separate approach / calibration would be needed.
I am grateful for any help or ideas to fix the issue !
Thanks a lot.
Cheers,
Thomas