Post Go back to editing

Self Test fails intermittently fails

Thread Summary

The user is experiencing ADXL367 self-test failures (diff > max or diff < min) in an embedded design. The final answer suggests adding a 100ms delay after entering Measure mode and averaging multiple samples to reduce noise. The user confirmed the issue persists with diff = 0 (x_axis_1 = 0xFFFF, x_axis_2 = 0xFFFF) and will verify if this is due to communication issues or other environmental factors. The ADXL367 is used in the design, and the self-test function is based on the Analog Devices reference code.
AI Generated Content
Category: Hardware
Product Number: ADXL367

Hello,

We are using ADXL367 in our design interfacing to our embedded microcontroller.

We have implented ADXL367 Self Test during initialization, but have seen cases where the test fails (diff > max OR diff < min). We have followed the Analog devices reference source code here, https://github.com/analogdevicesinc/no-OS/blob/main/drivers/accel/adxl367/adxl367.c


Max = 1080
Min = 360
Dif = ~700-800 (Happy Case)
Dif = 1678 (Failure Case, only failure data point I have for now)

Questions:

  1. Do you have any insight on what could cause these types of failures?


Our Self Test Function:

/***************************************************************************//**
 * @brief Performs self test.
 *
 * @param dev - The device structure.
 *
 * @return 0 in case of success, negative error code otherwise.
*******************************************************************************/
int adxl367_self_test(struct adxl367_dev *dev, int16_t* p_result)
{
	int ret;
	int16_t x_axis_1, x_axis_2, dif, min, max;
	uint8_t read_val;
	uint32_t st_delay_ms;

	// 4 / ODR value in ms
	/* TO give sensor enoug warm up time giving 500 ms delay. with 80 ms 
         * delay self test failing all time.
         */
        st_delay_ms = 500;
        /*
        switch (dev->odr) {
	case ADXL367_ODR_12P5HZ:
		st_delay_ms = 320;
	case ADXL367_ODR_25HZ:
		st_delay_ms = 160;
	case ADXL367_ODR_50HZ:
		st_delay_ms = 80;
	case ADXL367_ODR_100HZ:
		st_delay_ms = 40;
	case ADXL367_ODR_200HZ:
		st_delay_ms = 20;
	case ADXL367_ODR_400HZ:
		st_delay_ms = 10;
                break;
	default:
		return -EINVAL;
	}
        */

	ret = adxl367_set_power_mode(dev, ADXL367_OP_MEASURE);
	if (ret)
		return ret;

	ret = adxl367_reg_write_msk(dev, ADXL367_REG_SELF_TEST, ADXL367_SELF_TEST_ST,
				    ADXL367_SELF_TEST_ST);
	if (ret)
		return ret;
	// 4 / ODR delay
	OsDelayMs(st_delay_ms, OS_OPT_TIME_DLY);
	ret = adxl367_get_register_value(dev, &read_val, ADXL367_REG_XDATA_H, 1);
	if (ret)
		return ret;
	x_axis_1 = read_val << 6;
	ret = adxl367_get_register_value(dev, &read_val, ADXL367_REG_XDATA_L, 1);
	if (ret)
		return ret;
	x_axis_1 += read_val >> 2;
	// extend sign to 16 bits
	if (x_axis_1 & NO_OS_BIT(13))
		x_axis_1 |= NO_OS_GENMASK(15, 14);

	ret = adxl367_reg_write_msk(dev, ADXL367_REG_SELF_TEST,
				    ADXL367_SELF_TEST_ST_FORCE, ADXL367_SELF_TEST_ST_FORCE);
	if (ret)
		return ret;
	// 4 / ODR delay

	OsDelayMs(st_delay_ms, OS_OPT_TIME_DLY);
	ret = adxl367_get_register_value(dev, &read_val, ADXL367_REG_XDATA_H, 1);
	if (ret)
		return ret;
	x_axis_2 = read_val << 6;
	ret = adxl367_get_register_value(dev, &read_val, ADXL367_REG_XDATA_L, 1);
	if (ret)
		return ret;
	x_axis_2 += read_val >> 2;
	// extend sign to 16 bits
	if (x_axis_2 & NO_OS_BIT(13))
		x_axis_2 |= NO_OS_GENMASK(15, 14);

	ret = adxl367_set_power_mode(dev, ADXL367_OP_STANDBY);
	if (ret)
		return ret;

	ret = adxl367_reg_write_msk(dev, ADXL367_REG_SELF_TEST, 0,
				    ADXL367_SELF_TEST_ST_FORCE | ADXL367_SELF_TEST_ST);
	if (ret)
		return ret;

	dif = x_axis_2 - x_axis_1;
	min = ADXL367_SELF_TEST_MIN * adxl367_scale_mul[dev->range];
	max = ADXL367_SELF_TEST_MAX * adxl367_scale_mul[dev->range];
#if RTT_XL_DEBUG_OUTPUT
        SEGGER_RTT_printf(0, "  dif: %d\n", dif);
        SEGGER_RTT_printf(0, "  min: %d\n", min);
        SEGGER_RTT_printf(0, "  max: %d\n", max);
#endif

    // Copy result to output parameter
	*p_result = dif;

	if ((dif >= min) && (dif <= max)) {
		return  0;
	} else {
		return -1;
	}
}

Parents Reply
  • Hi Mario,

    We don't believe this to be the case as the command status is returning success, indicating the communication part worked ok.

    FYI, I would slap a Saleae analyzer on the I2C lines to confirm this, however the issue is only observed on an enclosed battery powered device. We do not encounter issue when attempting to replicate on evalutation.

    To confirm comm behavior, we can grab a Saleae trace using eval board to observe message timing and related.

Children
  • Hello  

    Thanks for the feedback. We would really appreciate it if you could cross-check it. That way, we can eliminate that source of the problem.

    Since you could only find this issue in the enclosed device, does this error occur consistently in different PCBs and sensors, or does it only occur in one?

    Regarding the device itself, could you verify any characteristics different from the test environment? Perhaps the battery is experiencing a voltage drop when the entire system tries to operate simultaneously. There may be signal integrity problems that could corrupt data. Alternatively, the mounting recommendations for the part may not have been followed, causing mechanical stress and inaccurate outputs.

    regards,

    Mario SM

  • Hi Mario,

    I learned sniffing SPI lines on the physical device is not possible. For now, we have added code to verify the return status of all commands within XL Self Test is valid.

    Also, we are looking to add a command that returns some type of data inside the XL Self Test to confirm that this works and not related to comm issue.

    I also learned XL Self Test always fails, even when commanded after initial power-on.

    We should be able to verify voltage level at least.

  • Please disregard previous message. I learned engineer performing testing was using older device with different XL model.

    We likely still have failures, but guess is the data will not be 0xFFFF.

    Will update when we have fresh data using correct hardware...

  • No problem, you are welcome.

    have a nice weekend,

    Mario SM

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.