Post Go back to editing

Output stability with capacitive load - required series resistor unclear

Thread Summary

The user inquired about the ADXL1003 MEMS sensor's requirement for a series resistor with capacitive loads larger than 100pF, noting a discrepancy with the recommended RC-filter values. The final answer suggests that for capacitive loads above 100pF, a series resistor of at least 500 ohm is needed, but no specific formula was provided. The ADXL1003 and ADAQ7980 were mentioned, with the RC-filter configuration using R=5kOhm and C=5nF for vibration measurements from 0 kHz to 5 kHz.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADXL1003

Hello,

I was reading up the ADXL1003 MEMS sensor datasheet (beause this part came up in the context of a running project).

Note 8 under Table 1 states that for capacitive loads larger than 100pF, a series resistor larger than 8kOhm must be connected. Yet page 11 recommends an RC-filter with R=5kOhm and C=5nF for vibration measurements from 0 kHz to 5 kHz. (With R2 being 0 and C2 not populated, the filter effectively becomes a simple RC. The amp in the ADAQ7980 is then configured as follower, i.e. has unity gain.)
What am I missing? Is the 8kOhm the minimum value to make the ADXL1003 output stable when the capacitive load is at the maximum allowed 22nF value? How to know the minimum required R for a given C?

Best regards,
Wim

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.