KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADXL1004
Recommended for New Designs
The ADXL1004 delivers ultralow noise density over an extended frequency range and is optimized for bearing fault detection and diagnostics. The ADXL1004...
Datasheet
ADXL1004 on Analog.com
ADXL1005
Recommended for New Designs
The ADXL1005 delivers ultralow noise density over an extended frequency range and is optimized for bearing fault detection and diagnostics. The ADXL1005...
Datasheet
ADXL1005 on Analog.com
Dear sir or madame,
we build up some three axis accelerometer based on your ADXL1004 and ADXL1005 mems sensors. In the intended application we now realized that there are high amplitudes at very high frequencies which activate the OR feature of the sensor. Unfortunatelly your implementation of the OR feature destroys the sensor signal instead of just informing with the dedicated OR-pin on the IC and simply clipping the signal at two times the nominal acceleration range.
So I have two questions to make the accelerometers usable in this application:
- Is there a possibility to disable the OR feature? Or at least disable the destruction of the sensor signal in case of OR?
- Do you have any experience in defined decoupling of the body vibrations with any kind of foam, rubber, ... which we can apply between the dut and our accelerometer? Frequencies above 10kHz and accelerations higher than 100g (and 500g) are not relevant for our analysis and could be damped away.
Many thanks and best regards,
Fabian
Hi flyget
yes, it is possible to disable the over-range protection feature. You need to pull high (VDD) the pin 21. Note that even though you can disable the over range protection feature, doing so it is at your own risk, as the sensor reliability qualification was performed with the over range protection enabled. The ADI recommended path would be to mechanically damp the vibration signature, as you mentioned with foam or rubber like materials, or plastic washers as well.
I hope this helps,
Pablo.
Hi Pablo,
thank you very much for the fast and positive reply! Do you recommend any pull up resistor for 5V VDD?
And yes, of course we have to look for the reliability, but I'm confident that we can solve the problem this way. First and fast step is that we will disable the feature and then have a look to reliability and mechanical damping.
Does your test and engineering team any recommodations about specific foam or rubber. Or any companys specialized in this kind of decoupling of body vibrations?
Best regards,
Fabian
Hi Fabian,
no need of pull up resistor.
I will ask our engineering team, but probably the answer is that we have not done any test on different materials to be able to recommend something in particular.
Regards,
Pablo
Hi Fabian,
no need of pull up resistor.
I will ask our engineering team, but probably the answer is that we have not done any test on different materials to be able to recommend something in particular.
Regards,
Pablo
Hi Pablo,
thanks!
I just tried your solution with binding Pin 21 to VDD, which seems working for us. Durability testing hasn't done yet, but for short term analysis is this a good solution up to now. First I wondered, as the OR-Pin is still indicating OR, but the signal isn't destroyed by it-> so everything good for us.
Are there other "hidden gems" which are not listed in the datasheet? *g*
Best regards,
Fabian