ADCMXL3021
Production
The ADcmXL3021 is a complete vibration sensing system that combines high performance vibration sensing (using micro-electromechanical systems (MEMS) accelerometers...
Datasheet
ADCMXL3021 on Analog.com
Dear All,
Recently, I encountered a Y-axis signal abnormality when using ADcmXL3021 in RTS mode for the first time.
Hardware: raspberry pi5b + ADCMXL_BRKOUT/PCBZ + ADcmXL3021
Register setting: REC_CTRL = 0x8103, RT_CTRL = 0x81
Enable SYNC/RTS function during execution (MISC_CTRL Bit12 = 1)
When using RTS mode, only the Y-axis signal is abnormal during the knock test (as shown in Fig. 1)

, and the Y-axis is abnormal when it is stationary (as shown in Fig. 2).

Can you provide the reason or is it a hardware damage?
Best
Chen