Hi.
The datasheet does not include dimensions for the pin headers of EVAL-ADXL345Z. Could you provide the dimensions for row-to-row distance and connector offset or Gerber files for this board so I can measure it myself?

Thanks.
ADXL345
Production
The ADXL345 is a small, thin, low power, 3-axis accelerometer with high resolution (13-bit) measurement at up to ±16g. Digital output data is formatted...
Datasheet
ADXL345 on Analog.com
Hi.
The datasheet does not include dimensions for the pin headers of EVAL-ADXL345Z. Could you provide the dimensions for row-to-row distance and connector offset or Gerber files for this board so I can measure it myself?

Thanks.
Hello Looongcat 
Here you can find some quick measurements. Currently we are not allowed to share the gerber files. (The EVB do not fit a regular breadboard in my experience)
Excuse the delay and hope this helps,
Mario SM
Hi Mario, and thank you for your reply.
Unfortunately, I can't open the two pictures you've attached. Could you re-upload them?
BR, Vasyl.
Excuse the inconvenient Looongcat
Taking as reference your image the distance between pins VIO and SCL is 1.25mm
for VS to INT2 8.875mm, I will edit the previous message, but it is already working on my side maybe some kind of bug.
Mario SM
Thanks, I'll stick with this values.