| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. Met after -8 hours |
RGrau DanB Akila mark.ramos mkhairy |
Open |
AD5940
Recommended for New Designs
The AD5940 and AD5941 are high precision, low power analog front ends (AFEs) designed for portable applications that require high precision, electrochemical...
Datasheet
AD5940 on Analog.com
pRampCfg->RampStartVolt = -1200.0f;
pRampCfg->RampPeakVolt = 400.0f;
pRampCfg->VzeroStart = 1500.0f;
pRampCfg->VzeroPeak = 1500.0f;
I have set these parameters in SWV, but I am still unable to see the oxidation of heavy metal ions. Here, if I am not wrong, the SWV ramp starts from 0.3V to 1.9V, but the metal ion oxidation is observed at negative potential. I have also tried to vary the potential ranges but can't optimize. I just want to know if there are any other parameters that need to be optimized that have a major effect on the metal ion oxidation.What parameters need to take care.Please help me.
lallison - Moved from StudentZone (Analog Dialogue) to Microcontroller no-OS Drivers. Post date updated from Monday, December 23, 2024 9:59 AM UTC to Tuesday, June 24, 2025 9:06 PM UTC to reflect the move.
Roht - Moved from Microcontroller no-OS Drivers to MEMS Inertial Sensors. Post date updated from Tuesday, June 24, 2025 9:06 PM UTC to Wednesday, June 25, 2025 2:08 PM UTC to reflect the move.