Post Go back to editing

Square wave voltammetry for heavy metal ion Detection

Thread Summary

The user is unable to observe the oxidation of heavy metal ions in SWV despite setting the ramp start and peak voltages. The final answer confirms the voltage range across the electrodes (CE and SE) is from -1.2V to 0.4V, suggesting the user check if the electrodes are correctly connected and verify the oxidation potential of the specific metal ions from standard tables.
AI Generated Content

pRampCfg->RampStartVolt = -1200.0f; 

pRampCfg->RampPeakVolt = 400.0f; 

pRampCfg->VzeroStart = 1500.0f; 

pRampCfg->VzeroPeak = 1500.0f;

I have set these parameters in SWV, but I am still unable to see the oxidation of heavy metal ions. Here, if I am not wrong, the SWV ramp starts from 0.3V to 1.9V, but the metal ion oxidation is observed at negative potential. I have also tried to vary the potential ranges but can't optimize. I just want to know if there are any other parameters that need to be optimized that have a major effect on the metal ion oxidation.What parameters need to take care.Please help me.

Thread Notes

Parents
  • Hi,

     Have you connected electrodes CE and SE across the electrolyte? 

    If so, with the above configuration, voltage across electrodes(VCE - VSE)  will vary from -1.2V to 0.4V.

     Depending on the metal and oxidizing agent, oxidation potential varies, whose values are listed in tables in internet.

Reply
  • Hi,

     Have you connected electrodes CE and SE across the electrolyte? 

    If so, with the above configuration, voltage across electrodes(VCE - VSE)  will vary from -1.2V to 0.4V.

     Depending on the metal and oxidizing agent, oxidation potential varies, whose values are listed in tables in internet.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.