In the ADXL357BEZ Rev A datasheet and on the product page's example circuit, the load on the V1P8ANA and V1P8DIG pins is a 0.1uF in parallel with a 1.0 uF capacitor.
However, the example circuit in the Rev C datasheet shows a 0.1uF capacitor in parallel with 100 K ohm resistor. There is wording that explains why the 100 K should be added:
"It is also highly recommended to help the LDO discharge properly by adding external resistors of approximately 100 kΩ between the LDO outputs (V1P8ANA and V1P8DIG) and ground (0 V), especially when power cycling at temperatures below −20℃."
Does there still need to be a 1 uF capacitor on the LDO outputs? Or has the internal regulator itself changed so that it is no longer required?