ADXL314
Recommended for New Designs
The ADXL314 is a ±200 g range, 13-bit resolution, 3-axis digital accelerometer. The digital output data is formatted as 16-bit, twos complement data and...
Datasheet
ADXL314 on Analog.com
What are the scaling factor of ADXL314 at 3200 ODR ?
Hi ADXL314 thanks for your question.
For this part the scale factor remains the same on its different ODR configurations.
Do not hesitate to ask for further assistance in case you need it.
Regards,
Mario SM
What is the maximum resolution we can achieve in terms of G.
Hello back again,
We can calculate the resolution taking in account the Measurement range and the output resolution:
Which equals to the scale factor ( 1/ scale factor in g will give us the 20.48 sensitivity value)
Also we could take in account noise factors due to different ODR, or a typ (68% population) 10% calibration error as noted in the datasheet.
On the ODR side we can expect a peak (99.9% population) noise value of 0.965 g at 3200 Hz ODR.
Hope this helps,
Mario SM
Hello Marlo,
Thanks for the detailed answer
Can you share the longevity of this product or when it will be out of production
Hello Marlo,
Thanks for the detailed answer
Can you share the longevity of this product or when it will be out of production
Hello ADXL314
We have no long-term plans to discontinue this part.
Hope this solves your question,
Mario SM