Post Go back to editing

ADXL314

Thread Summary

The user asked about the scaling factor of the ADXL314 at 3200 ODR. The support engineer confirmed that the scale factor remains constant across different ODR configurations. The maximum resolution is 0.488 g, and the peak noise value at 3200 Hz ODR is 0.965 g. The product has no planned discontinuation.
AI Generated Content
Category: Hardware
Product Number: ADXL314

What are the scaling factor of ADXL314 at 3200 ODR ?

Parents Reply
  • Hello back again,


    We can calculate the resolution taking in account the Measurement range and the output resolution:

    \frac{400}{2^{13}}=0.488\text{ g}

    Which equals to the scale factor ( 1/ scale factor in g will give us the 20.48 sensitivity value)

    Also we could take in account noise factors due to different ODR, or a typ (68% population) 10% calibration error as noted in the datasheet. 

    On the ODR side we can expect a peak (99.9% population) noise value of 0.965 g at 3200 Hz ODR.

    Hope this helps,

    Mario SM

Children