Post Go back to editing

Measuring acceleration data using Nidaq 6323

Category: Hardware
Product Number: ADXL358
Hi
I'm trying to use Nidaq 6323 to read the acceleration data from ADXL358. Since Nidaq directly reads analog signal as voltage, I'm facinf issues with interfacing the accelerometer with the daq. I notice that when I divide the measured voltage with the sensitivity then all the three axes are reporting ~11 (Raw_voltage/sensitivity: 1V/0.08=10g?). Even when I place the accelerometer on a flat surface I get the same reading.
 
(Note: I have set the range as +/- 10g, put both the ST1 and ST2 pins to low and STBY to high)

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.