Post Go back to editing

Feedback Request for ADXL327 Schematic and PCB Design – Sensitivity Asymmetry and System Improvement

Category: Hardware
Product Number: ADXL327
I'm currently working on a project using the ADXL327 accelerometer connected to an INA126 differential amplifier, with the system powered by 3.3V. My goal is to achieve highly accurate G-value readings, but I'm noticing an asymmetry in the sensitivity between +G and -G measurements, which affects my results.
  • Open Circuit Setup (Amplifier Disconnected):
  1.  +1G Output: 2.128V; Sensitivity: 0.478 mV/G (from 2.128V - 1.65V)
  2.  -1G Output: 1.189V; Sensitivity: 0.461 mV/G (from 1.65V - 1.189V)
  • Connected to Differential Amplifier (INA 126) (X-Axis Output Connected):
  1. +1G Output: 2.079V; Sensitivity: 0.429 mV/G (from 2.079V - 1.65V)
  2. -1G Output: 1.191V; Sensitivity: 0.459 mV/G (from 1.65V - 1.191V)
These indicate a slight asymmetry in sensitivity for both setups, which I would like to address.
 
Attached Files:
  1. Schematic Diagram – Showing the ADXL327 connection to the INA126.
  2. PCB Layout – Illustrating the component placement, trace routing, and grounding. 
Additional Notes:
  • Supply Voltage: System is powered with 3.3V.
  • Single-Axis Requirement: My application requires only one axis, so I’m currently using the X-axis.
  • Component Note: R24 is marked DNP (Do Not Place) and is not present in the circuit.
  • INA126 Input Impedance: The input impedance of the INA126 is very high, specified as 10⁹ Ω in the datasheet, which should minimize loading effects on the accelerometer.
  • Accelerometer Output: The ADXL327 output is connected only to the INA126 input and a test point; it is not connected to any other circuitry.
 
Question:-
Achieving Symmetric Output: How can I adjust the circuit to achieve more symmetric output between +G and -G to improve the accuracy of my G-value measurements?