Post Go back to editing

Accelerometer Zero-g offset temperature drift Upper limit standard

Category: Datasheet/Specs

I'm doing zero-g offset temperature verification on several Accelerometers. I noticed in the documentation that the Zero-g offset temperature drift for the Accelerometersis ±0.2 mg/°C (Figure 1).

My question is: I am testing the Zero-g offset temperature drift in a temperature chamber from -20°C to 85°C (with a zero calibration performed at 25°C beforehand)Figure 3. What are the upper and lower limits for determining a Fail in terms of the offset? How is it calculated? What is the reference standard?

Should I calculate the limits as (20 + 85 = 105), 105 * 0.0002g = 0.021g as the standard for the upper and lower limits?
Or should I use Zero-g offset (including temperature and lifetime effects) = 20 mg as the standard for the limits?
Thank you!

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.