Post Go back to editing

Accelerometer Zero-g offset temperature drift Upper limit standard

Category: Datasheet/Specs

I'm doing zero-g offset temperature verification on several Accelerometers. I noticed in the documentation that the Zero-g offset temperature drift for the Accelerometersis ±0.2 mg/°C (Figure 1).

My question is: I am testing the Zero-g offset temperature drift in a temperature chamber from -20°C to 85°C (with a zero calibration performed at 25°C beforehand)Figure 3. What are the upper and lower limits for determining a Fail in terms of the offset? How is it calculated? What is the reference standard?

Should I calculate the limits as (20 + 85 = 105), 105 * 0.0002g = 0.021g as the standard for the upper and lower limits?
Or should I use Zero-g offset (including temperature and lifetime effects) = 20 mg as the standard for the limits?
Thank you!

Parents Reply
  • Hello, I am responsible for a department that is currently conducting temperature drift validation on ADI's ADXL354 and another sensor from Bosch, the SMI230. I would like to first understand the validation standards for the ADXL354, as this should give me a clearer understanding of how to validate accelerometers. Thank you for your help!

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.