Post Go back to editing

ADIS16480 test conditions of Static and Dynamic Accuracy value

Thread Summary

The user inquired about the static and dynamic accuracy values of the ADIS16480's yaw, pitch, and roll angles. The dynamic accuracy is tested using a sinusoidal angular rotation of 30 degrees peak-to-peak at 0.6 Hz, with 4 cycles over a 10-second window. The sensor samples data at 1200 SPS, and the dynamic accuracy is determined by the standard deviation of the angular position error.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADIS16480

Hi sir

According to the datasheet, The static accuracy of the ADIS16480's yaw angle is 0.3 degrees, and the roll and pitch angles are 0.1 degrees. The dynamic accuracy of the yaw angle is 0.5 degrees, and the roll and pitch angles are 0.3 degrees.

I would like to know how these values are obtained and whether they are based on any relevant international standards, or if there are any related tests(include both static and dynamic testing)?

I have read the following article 'ADIS16480 test conditions of Dynamic Accuracy value', but I don't understand the meaning of '4 cycles @ 0.6Hz.' Does it refer to a sine wave with 4 cycles and a frequency of 0.6Hz? If so, the total time would be less than 10 seconds, which seems to contradict the 'measured over 10 sec window' statement.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.