Post Go back to editing

Can't read Prod ID on Esp32S3

Category: Software
Product Number: ADIS16505-3
Software Version: Latest

Hi all,

Hardware:

adis16505-3

Esp32-S3-wroom-2

Issue:

I'm running into trouble trying to read the Prod Id I'm just getting all 0's out. I have the IMU on the SPI2 pins and set up the SPI channel at 1MHz. I initially created the SPI cmd as described in the data sheet as:

uint16_t tx_data = (0 << 15) | (reg_addr << 8 );

But I noticed on the scope that the DIN line seemed to be shifted to the right, see the second picture against the 3rd picture.

I tried switching it to

uint16_t tx_data = reg_addr;

not shifting it at all and that produced a scope perfectly resembling the data sheets example, see the last picture.

Code:

Reading register : 0x72

SPI Config:

    spi_bus_config_t buscfg = {

        .miso_io_num = PIN_NUM_MISO,

        .mosi_io_num = PIN_NUM_MOSI,

        .sclk_io_num = PIN_NUM_CLK,

        .quadwp_io_num = -1,

        .quadhd_io_num = -1,

        .max_transfer_sz = 4 * 1024

    };

    spi_device_interface_config_t devcfg = {

        .clock_speed_hz = 1 * 1000 * 1000, // 1 MHz to meet timing requirements

        .mode = 3,                         // SPI mode 3 (CPOL=1, CPHA=1)

        .spics_io_num = PIN_NUM_CS,

        .cs_ena_pretrans = 8,              // Ensure CS is activated 8 SPI clock cycles before transmission

        .cs_ena_posttrans = 8,             // Ensure CS stays active 8 SPI clock cycles after transmission

        .input_delay_ns = 25,              // Based on tDAV and tDSU requirements (typical 25 ns)

        .queue_size = 3

    };

Reading attempt:

esp_err_t imu_read_register(spi_device_handle_t spi, uint8_t reg_addr, uint16_t *data) {

    uint16_t tx_data = (0 << 15) | (reg_addr << 8); // Read command (0), followed by the 7-bit address and 8 don't care bits

    uint8_t rx_buffer[2] = {0x00, 0x00};

    spi_transaction_t t;

    memset(&t, 0, sizeof(t));

    t.length = 16;            // 16 bits for the transaction

    t.tx_buffer = &tx_data;

    t.rxlength = 16;          // 16 bits to read

    t.rx_buffer = rx_buffer;

    esp_err_t ret = spi_device_transmit(spi, &t);

    if (ret == ESP_OK) {

        *data = (rx_buffer[0] << 8) | rx_buffer[1];

        ESP_LOGI(TAG, "Read from register 0x%02X: 0x%04X", reg_addr, *data);

    } else {

        ESP_LOGE(TAG, "Failed to read register 0x%02X: %s", reg_addr, esp_err_to_name(ret));

    }

    return ret;

}


I only have a 2 channel scope so forgive the fragmentation of this snippets.

CS over SCLK

SCLK over DIN : Here you can see DIN is shifted to the right of what it should be


Data sheet example



SCLK over DIN: Shifted to the left matching the data sheet

No matter what I try though I always get 0's from DOUT.

Are there any examples using the espressif toolchain I could reference?

*Separate question: I looked at the analog GitHub and it has a driver library for the 164X, I was wondering if there's an updated one for the 16505 available?

Best Regards,

Wade

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.