When using the CAPTURING IMPACT EVENTS feature of the ADXL372 for peak detection, what is the minimum value that can be set for the activity threshold? When setting the activity threshold to 2g, peak detection does not occur.
ADXL372
Recommended for New Designs
The ADXL372 is an ultralow power, 3-axis, ±200 g MEMS accelerometer that consumes 22 µA at a 3200 Hz output data rate (ODR). The ADXL372 does not power...
Datasheet
ADXL372 on Analog.com
When using the CAPTURING IMPACT EVENTS feature of the ADXL372 for peak detection, what is the minimum value that can be set for the activity threshold? When setting the activity threshold to 2g, peak detection does not occur.
Hi Yukio ,
The minimum would be slightly higher than 3g. I added below the limitations section of the ADXL372 section explaining why that is the case.
Thanks,
Marine ()
Hi Marine,
Thank you. I understand.
Yukio