Post Go back to editing

MSL Level

Thread Summary

The user inquired about the moisture sensitivity level (MSL) for the ADIS16460AMLZ, which is not rated for solder reflow processes due to its connector-based attachment. The final answer clarifies that the device does not have an MSL rating as it is not applicable.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADIS16460AMLZ, ADIS16460

What is the MSL level for ADIS16460AMLZ?  I don't  see it listed in the data sheet.  

  • Thank you for the interest in the ADIS16460. 

    By "ML," are you referring to the moisture level, per JEDEC J-STDD-033?

    If so, my understanding is this only applies to devices that are attached via solder reflow processes, such as those in J-STD-020. 

    The ADIS16460 attaches via connector and is NOT rated for such exposure. 

    This is why there is no moisture level rating. 

    Does that help?