Post Go back to editing

ADXL1001BCPZ fails when Z force is about 200g

Thread Summary

The user experienced a failure of the ADXL1001 accelerometer after exposure to 200g centripetal forces along the Z-axis while measuring up to 100g on the X-axis. The support engineer suggested checking Analog Devices' parametric search tool for accelerometers capable of withstanding higher Z-axis forces. The user noted the presence of analog options in the search results.
AI Generated Content
Category: Hardware
Product Number: ADXL1001BCPZ
Software Version: N/A

I am using an ADXL1001 inside a propeller hub to measure forces along rotational axis. The ADXL1001 is specified to handle forces up to 100g along the X-axis. Inside the hub it is also subject to centripetal forces of about 200g along the Z-axis. The sensor was working properly until it experienced the 200g force along the Z-axis and then it seems to have jammed. The neutral value on my ADC pin is 2048 (maximum 4095) and I am now just getting a low signal of about 1000. It may be that this sensor is unsuitable for a situation with a high Z-axis force. Is there any sensor capable of withstanding 200+ on Z-axis, and measuring up to 100g on the X-axis?

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.