Newbie questions:
I have an EVAL-ADXL367-SDP customer evaluation system as shown here. The associated software customer evaluation SW has been installed on a Windows 10 computer. After connecting the boards via USB, opening the SW tool, entering the Rev board option (Rev. 4), and clicking on the Start Data Acquisition button, I see a completely flat line for the X,Y, and Z accelerations pegged at -0.0025g. The curves never deviate from this level even in response to device motion. How can I get this to work as expected? Also, the weblink shows a demo tab which doesn't appear on my version. How can I bring up the demo tab?
Thanks.
I've attached photos of the setup as well as a screenshot of the tool.

dsf