Dear members,
I am looking for information on ADXL202, ADXL210, and ADXL345's built-in filtering to determine if and what kind of signals could be attenuated by this internal filtering.
Any feedback would be much appreciated.
Thank you!
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
ADXL202
Obsolete
Please see the ADXL203.
The ADXL202E is a low-cost, low-power, complete dual-axis iMEMS® accelerometer with a measurement range of ±2g. The ADXL202...
Datasheet
ADXL202 on Analog.com
ADXL210
Obsolete
The ADXL210 is a low cost, +/-10 g, dual-axis iMEMS® accelerometer with a digital output, all on a single monolithic IC. The ADXL210 will measure accelerations...
ADXL210 on Analog.com
ADXL326
Production
The ADXL326 is a small, low power, complete 3-axis accelerometer with signal conditioned voltage outputs. The product measures acceleration with a minimum...
Datasheet
ADXL326 on Analog.com
ADXL345
Production
The ADXL345 is a small, thin, low power, 3-axis accelerometer with high resolution (13-bit) measurement at up to ±16g. Digital output data is formatted...
Datasheet
ADXL345 on Analog.com
Dear members,
I am looking for information on ADXL202, ADXL210, and ADXL345's built-in filtering to determine if and what kind of signals could be attenuated by this internal filtering.
Any feedback would be much appreciated.
Thank you!
I am so sorry for the late reply. ADXL202 and 210 lifecycles are obsolete (The models in this product family are no longer available). There are suggested replacement parts (ADXL212 instead of ADXL202, and ADXL326 instead of ADXL210). Please check them if they can meet your application requirements.
Regarding the ADXL345, please check the attached photo, which displays the low-pass filter data at different output data rates.

Regards,
Mohammad
Hi Mohammad, thanks for your answer! I am in fact looking for info on these "obsolete" models so I can understand some 'old' data collected with such older devices! I appreciate your help and the images you provided.