Hi team,
Our customer is measuring 0g voltage temperature drift on the Z axis.
As a result, the output voltage of all the measured samples decreased in proportion to the temperature.
It varies more than 100mV from minimum to maximum temperature range.
On the other hand, the datasheet gives the following graph as reference data.

Our customer's result changes linearly over 100mV with a temperature change of 100°C.
I feel that the amount of change is large compared to the graph above.
The graph above is centered at 30°C.
Is it possible that variation causes the output voltage to drop in a first order line instead of this graph?
Please let me know if there are any special measurement conditions.
Best regards,
T-yoshi