The ADXRS645 has a default range of ±2000 °/sec and a scaling of 1 mV/°/sec which equates to 0.5V to 4.5V centred around 2.5V. If the ±5000 °/sec option is implemented is full scale still 0.5V and 4.5V. Or should I use 0V and 5V?
Kind Regards
Martin
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADXRS645
Recommended for New Designs
The ADXRS645 is a high performance angular rate sensor with excellent vibration immunity for use in high temperature environments. The ADXRS645 is manufactured...
Datasheet
ADXRS645 on Analog.com
The ADXRS645 has a default range of ±2000 °/sec and a scaling of 1 mV/°/sec which equates to 0.5V to 4.5V centred around 2.5V. If the ±5000 °/sec option is implemented is full scale still 0.5V and 4.5V. Or should I use 0V and 5V?
Kind Regards
Martin