(1) Does the /CS pin need to be High/Open to start DR output?
The datasheet states that the DR signal is output after the START-UP TIME after the ADIS16500 is powered on. (Figure 29)
When I looked at the waveform on the oscilloscope, when I turned on the ADIS16500,
・/CS Low => DR signal output does not start
・/CS High or Open => DR signal output starts
You can see the above phenomenon.
According to the specifications of the ADIS16500, is it true that DR output will not start unless /CS is High/Open when the power is turned on?
(If possible, could you confirm the reason?)
(2) Is it okay to write/read registers while DR is inactive?
It states that you should read the Gyro and Accel registers while DR is Active.
Non-measured registers such as Product No. and MSC_CTRL
Does DR need to be Active even when writing or reading?
We apologize for the inconvenience, but thank you for your kind support.