For the temperature sensor specifications of the ADIS16500,
Please allow me to confirm two points.
Q1:
"TEMPERATURE SENSOR" on page 4 of the data sheet says
It says "Output = 0x0000 at 0°C (±5°C)".
Does this mean that the temperature sensor accuracy is about ±5°C?
If possible, I would like to ask for a guideline for the accuracy of the temperature sensor.
Q2:
On page 16 of the data sheet, the angular velocity and acceleration
There is a description of CALIBRATION.
(Excerpt below)
"at multiple temperatures over the calibration temperature range
(-40°C <= TC <= +85°C)."
Is it correct to interpret that FACTORY CALIBRATION also performs temperature correction based on the values obtained from the temperature sensor in the ADIS16500?
Or does it mean that the temperature is corrected based on an external temperature sensor (such as a thermometer in a constant temperature bath)?