Post Go back to editing

AXDL355 Activity Detection Enable

Category: Choose a category
Product Number: ADXL355

I want to know if I want to enable activity detection, what value 1 or 0 I shall set for x, y, z bi in ACT_EN register (0x24).

The data sheet only says 0 for reset. Reset means disable? And 1 for enable?

Another issue:

For INT polarity, what does "active 0" mean? Is it that if interrupt occurs, the pin goes from Hight to Low?



Need clarification for interrupt pin polarity
[edited by: DJSG at 9:52 AM (GMT -4) on 22 Sep 2022]

Top Replies

    •  Analog Employees 
    Nov 17, 2022 in reply to DJSG +2 verified

     Hi  , 

    I see that in your configs is not the INT_MAP register (0x2A). 

    this register needs to be configured to map the desired interrupt pin. 

    I hope this helps, 

    Pablo 

Parents Reply Children
No Data