ADXL327
Production
The ADXL327 is a small, low power, complete 3-axis accelerometer with signal conditioned voltage outputs. The product measures acceleration with a minimum...
Datasheet
ADXL327 on Analog.com
ADXL372
Recommended for New Designs
The ADXL372 is an ultralow power, 3-axis, ±200 g MEMS accelerometer that consumes 22 µA at a 3200 Hz output data rate (ODR). The ADXL372 does not power...
Datasheet
ADXL372 on Analog.com
We are using the EVAL-ADXL372Z connected to and powered by ESP32 dev board. SPI rate is 10 MHz.
The eval board is powered by the ESP32 dev board (which has a AMS1117-3.3 1A LDO, powered by PC’s USB VBUS).
The entire test setup in on the ground, away from any shock/vibration sources.
The sensor is set to Full bandwidth mode and the samples are read through the serial port.
We are experimenting with different sample rates to measure noise performance of the ADXL372. We see noticeable noise power at ~80 Hz (for 400Hz & 800Hz sampling rate) on all three axes in our fft graphs. Do you have any explanation for this noise? Can you suggest some experiments to help us determine the source of this noise?