I have an ADIS16505 IMU connected to a microcontroller. I have been working with these devices successfully for several years. I have seen where the device is working properly and then begins to produce zero data on all six IMU devices. I am requesting data at 100Hz and using the synch pin to synch sampling with GPS 1PPS (one/sec). I use the DataReady to provide an interrupt to the microcontroller to produce a "Burst Read" of the 16bit data words both the low and high words for all devices. Generally all this seems to work just fine. Once the IMU starts producing the zero data -- it doesnt recover.
Any thoughts on the internal mechanism that would produce zeros from the IMU?
Jim Kain 781 856 6175