Our product use the ADXL354 and use the self test.
The self test output variation(Z-Axis) is 0.5g - 3.0g(Typ:1.5g).
The self test output variation(X,Y-Axis) is 0.1g - 0.6g(Typ:0.3g).
We think that the self test output variation is large.
However, we checked the self test output value and the value is about typical value.
What is the variation factor? (Lot variation?)