Post Go back to editing

Which LDO is suitable for ADXL354?

Thread Summary

The user asked about using a 3.3V LDO for VCC or a 1.8V LDO for V1P8ANA in a low noise circuit design with the ADXL354. The final answer indicates that using a 1.8V LDO for V1P8ANA is better, but the difference is minimal. The design team clarified that the sensor and front-end amplifier are the primary noise sources, and using a low-noise external LDO does not significantly improve noise performance beyond the internal regulated supply.
AI Generated Content

Hello everyone~
I have an ADXL354 and I am designing a low noise circuit. May I ask if I should use 3.3VLDO to supply VCC of ADXL354 or 1.8VLDO to supply V1P8ANA of ADXL354?
Last question, can you recommend a low noise external LDO for ADXL354?
my power supply is 5V I am using ADR4550 as reference voltage.

Thanks for your replies.

Edit Notes

I am using ADR4550 as reference voltage.
[edited by: yaro-0916 at 3:37 PM (GMT -4) on 2 Apr 2022]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.