Post Go back to editing

ADXL355 sample rate tolerance

I recently completed a 23 day study comparing the ADXL355 to a very high end accelerometer from another company.  The ADXL performed very well in terms of magnitude and reliability.  In order to match the other accel we had to adjust the set sample rate of the unit.  We needed to adjust it by +1.2% which seemed very high.  I looked through the spec for a tolerance on the internal clocks but I didn't see something I could convert to allowable tolerance on the rate.  The rate was very consistent so I don't think there is internal drift.  I am curious what the tolerance of the frequency setting is.

Parents
  • Thank you for your post.  I am sorry for the delay in our response.  We are on holiday this week, but I can say that I was able to find some original design documents, which projected a tolerance of +/-2% and that the temperature variation, over -40C to +125C, would be less than 3%.  I have not been able to find any drift metrics on this metric, but 1.2% sounds fairly high, assuming the 23 days were under "normal use" conditions, rather than accelerated aging profiles. 

    FormerMember - When you return, can you comment if you have any additional information on this metric? Thank you! 

Reply
  • Thank you for your post.  I am sorry for the delay in our response.  We are on holiday this week, but I can say that I was able to find some original design documents, which projected a tolerance of +/-2% and that the temperature variation, over -40C to +125C, would be less than 3%.  I have not been able to find any drift metrics on this metric, but 1.2% sounds fairly high, assuming the 23 days were under "normal use" conditions, rather than accelerated aging profiles. 

    FormerMember - When you return, can you comment if you have any additional information on this metric? Thank you! 

Children