ADXL 362 Anti-Aliasing clarification

Hello,

I am currently using the ADXL 362 for motion detection and wanted a quick clarification on the Anti-aliasing filters. I intend on using the device in loop-mode with no wake-up mode. Specifically I want to be able to detect shock events at the 400Hz range instead of the wake-up mode 6Hz. Does the anti-aliasing apply to this detection?

The function block diagram implies that this is the case, but I just wanted to get clarification on this before depending on this sample rate for a specific shock detection capability. Is the 6Hz wake-up mode detection also anti-aliased?

Parameters I am setting is: 400Hz ODR, 1/2 bandwidth, loop mode, referenced detection, and no wake-up or autosleep mode/ measurement mode only.