1) In datasheet 'Linear Acceleration Effect' for all axes is provided. Since it is a gyro which is mostly measuring the rotational rate, can you provide test data for 'Angular' acceleration effect for the remaining rotational axes?
2) May I know 'Vibration Rectification' parameter mentioned in the datasheet is for which axis?
3) Sensor Resonant Frequency parameter mentioned in the text is 17.5KHz whereas from the Figure 15, the same looks like it is 1.75KHz. Can you confirm which is right?
4) Can you provide the transfer function of the sensor? In Figure 15 of datasheet, magnitude and phase response for Cout = 470pF is provided. We want to determine the magnitude and phase response for a different value of Cout.
5) Do you have any test results that show the effect on measured Z axis gyro rate due to coupling from angular rotations in Y axis and X axis?