Post Go back to editing

ADIS16201 use with FX3 Sensor Evaluation Systems board

Thread Summary

The user inquired about connecting an ADIS 16201/PCB daughter board to an ADI FX3 Sensor Evaluation Systems board using a 2x8 ribbon cable. The solution is to connect ADIS16201/PCBZ J1-Pin1 to EVAL-ADIS-FX3 P3-Pin1, which results in pins 13, 14, 15, and 16 of J1 not being connected. The user confirmed that this solution was derived from the schematics and that the provided picture clarified the connection, despite initial confusion.
AI Generated Content

I have an ADIS 16201/PCB daughter board and an ADI FX3 Sensor Evaluation Systems board to test an ADIS 16201 accelerometer chip.  I do not see how to connect the two boards together with the provided 2x8 ribbon cable.  The 16201/PCB has two 2x6 connectors.

Parents
  • Thank you, , for sharing this!  We are sorry about the confusion.  

    ADIS16201/PCBZ - J1-Pin1 connects to P3-Pin1, on the EVAL-ADIS-FX3.  This will cause the ribbon connector to have pins 13, 14, 15 and 16 NOT connected, on J1 (ADIS16201/PCBZ), since it only has 12 pins.  The following picture shows one of the ADIS16505x-x/PCBZ, but with some physical markers, for identifying the connection and expected, connector over-hang. 

    Does this help? 

Reply
  • Thank you, , for sharing this!  We are sorry about the confusion.  

    ADIS16201/PCBZ - J1-Pin1 connects to P3-Pin1, on the EVAL-ADIS-FX3.  This will cause the ribbon connector to have pins 13, 14, 15 and 16 NOT connected, on J1 (ADIS16201/PCBZ), since it only has 12 pins.  The following picture shows one of the ADIS16505x-x/PCBZ, but with some physical markers, for identifying the connection and expected, connector over-hang. 

    Does this help? 

Children