Post Go back to editing

ADIS16470 - exceeding 40 g

Hello,

I am building a model rocket for an extracurricular project at my school and the rocket will peak at 60 (!) g of acceleration. I wanted to know if the behaviour of the ADIS16470 IMU or any other 40 g accelerometer for that matter was known after it has saturated. Once the acceleration reduces underneath its maximum of 40 g, does it behave normally? Or does it have a sort of bias that would need to be accounted for afterwards? I am currently torn between using this IMU as-is or rotating it to be angled to split the 60 g of acceleration evenly between all three axis and therefore bringing it under 40 g.

Additionally, if someone had any advice or could point me towards a better solution where I wouldn't run into this limit. Perhaps if another known IMU can handle the 60 g of acceleration, or if I would be better off using a 3-axis accelerometer and gyroscope triad separately.

Thank you!

Joshua

Parents
  • Hi ,

    Sorry for the late response. 
    Here's a snippet from the datasheet:

    ABSOLUTE MAXIMUM RATINGS

    Table 3. Parameter Rating

    Mechanical Shock Survivability
    Any Axis, Unpowered 2000 g
    Any Axis, Powered 2000 g

    Stresses at or above those listed under Absolute Maximum Ratings may cause permanent damage to the product. This is a stress rating only; functional operation of the product at these or any other conditions above those indicated in the operational section of this specification is not implied. Operation beyond the maximum operating conditions for extended periods may affect product reliability.

    As for now, our IMUs have a max. acceleration range of 40g. 

    Hope this helps. 

    Best regards,
    John

Reply
  • Hi ,

    Sorry for the late response. 
    Here's a snippet from the datasheet:

    ABSOLUTE MAXIMUM RATINGS

    Table 3. Parameter Rating

    Mechanical Shock Survivability
    Any Axis, Unpowered 2000 g
    Any Axis, Powered 2000 g

    Stresses at or above those listed under Absolute Maximum Ratings may cause permanent damage to the product. This is a stress rating only; functional operation of the product at these or any other conditions above those indicated in the operational section of this specification is not implied. Operation beyond the maximum operating conditions for extended periods may affect product reliability.

    As for now, our IMUs have a max. acceleration range of 40g. 

    Hope this helps. 

    Best regards,
    John

Children
No Data