ADXL362 FIFO writing time

Hi

I am FAE in Japanese distributor.

Our customer use ADXL362.

ODR of ADXL362 is 12.5Hz and FIFO is assigned 125bits.

INT1 is assigned Water Mark Bit (Register 0x2A=0x04).

The following picture shows 11.8 seconds of INT1 "L" period.

It only takes 10s(125x1/12.5) to write 125bits FIFO.

How many cycles does it take to start writing to next FIFO after clearing INT1("H " to "L")?

How many cycles does it take to assert INT1("L" to "H") after finishing to write 125bits FIFO?

Is there a possibility that the above time will change by about 1 second?

Best regards

N.Kokubo



ADX to change ADXL362
[edited by: NKokubo131 at 1:52 AM (GMT -4) on 28 Oct 2020]

Top Replies

Parents Reply
  • +1
    •  Analog Employees 
    on Nov 5, 2020 11:44 AM 3 months ago in reply to NKokubo131

    Hi ,

    They may base on the datasheet for that matter:

    So as you can see here, since the ADXL362 can operate with external frequencies ranging from the nominal 51.2 kHz down to 25.6 kHz, the customer has 2 options to achieve this. 
    Basing on the Filter Control Register:

    Option 1: 

    Set 000  on bits [2:0] on the Filter Control register and then provide a 51.2 kHz external clock. This would result to:

    Option 2: 
    Set 001 on bits [2:0] on the Filter Control register and then provide a 25.6 kHz external clock. This would then result to:

    Hope this helps! 

    Best regards,
    John

Children