Post Go back to editing

ADXL213 Dynamic Anglog measuring method

In the early stage, I used the ADXL213 sensor to build a circuit to realize the Angle of inclination. Since the installation is not from the center of the circle, the Angle of inclination fluctuates within the range of 0° to 20° in the process of non-uniform motion.What kind of gyroscope should I add to match with the original ADXL213 so that the scheme can be realized?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.