Post Go back to editing

EVAL-ADXL344Z-DB Board SW Project and XLS missing

Hello, 

EVAL-ADXL344Z-DB is a perfect tool to research on pedometers, movement logging and similar. 


According to user guide UG-065 there must be a XLS sheet for data plotting.
As well as a Keil project datalogger.uvproj. Probably suppoted at MDK 4.11.

I can't find any files on the evaluation board page, nor at product page.

Could you please let me know how I can download these?

Thanks and best regards

Parents Reply Children
  • Just for clarification...I am also searching for the source code to program the micro controller on the adxl345z-eval. When I follow the link provided above and click on the zip file "EVAL-ADXL34xZ-DB Evaluation Software" it does not contain any source code.

    According to UG-065: SOFTWARE TOOLS In addition to the ready-to-upload examples provided in the Firmware link of the Development Board section of the ADXL345 product page, the development board is fully modifiable and reprogrammable to allow for easy prototyping and firmware development. Firmware is written in C, and it is compiled for the ADuC7024 ARM7 processor. The firmware examples provided on the ADXL345 product page were written using Keil Microvision and compiled using the RealView compiler. A free evaluation version of Keil Microvision is available online. Additional software suites (Keil, IAR, and GNU) for writing and compiling code are available. For instructions on how to install and use the software, refer to the ADuC702x MicroConverterTm GetStarted Guide. To reprogram the board, download the ARMWSD program from the Uploader link in the Development Board section of the ADXL345 product page. When Keil Microvision is installed, complete the following steps: 1. Click and download the Sample Project (EVALADXL345Z-DB Files.zip) file from the ADXL345 Development Board section of the ADXL345 product page. 2. Unzip the EVAL-ADXL345Z-DB Files.zip file into a known directory. 3. Navigate into the EVAL-ADXL345Z-DB folder and open datalogger.uvproj. This Keil Microvision project allows users to modify and recompile the program. 

    Where can I locate the source code for the sample project and the datalogger.uvproj?

    Thanks,

    JC

  • Hi  , 

    Attached is the source code. 

    Regards, 

    Pablo. 

     8816.EVAL-ADXL345Z-DB Files.zip