Post Go back to editing

Zero characteristic of ADXRS453

Hello! When I used the ADXRS453 device, I found that in the temperature range of -40℃~80℃, the static output data changes irregularly, and it cannot be compensated better. Is it my problem? When describing its zero output accuracy in the device manual, it is said as "0.4/sec @25℃. Is it true that a piece of ADXRS453 will change its static output within 0.4/sec when it is energized for many times at normal temperature?