Hello,
I work with a drone company and we are testing the use of ADIS16448 in our products. Normally, with other ADIS products (such as ADIS16405), we calibrate the magnetometers for Hard Iron and Soft Iron effects, and only need to recalibrate every 100 flights.
However, in our tests with ADIS16448 and the same usual hardware, we have observed that calibration is lost right after a few flights (5 or so). In some cases, we have observed calibration losses overnight, without even having flown.
We believe that we have made the appropriate hardware adaptations (e.g. power supply reduction from 5V to 3.3V) for it to work properly. Due to dimensional differences between the ADIS16405 and the ADIS16448, the ADIS16448 mounting in our hardware is now closer to our GNSS (right under it). The rest of the distances between hardware components haven't changed significantly. We 3D-printed a bracket for the IMU made of ABS and fixed it to our hardware using stainless steel nuts and screws.
Could you provide me some information if this change in magnetometer calibration stability from one ADIS product to the other is expected?
Thanks you in advance,
Tomas