Post Go back to editing

Performance of MEMS accelerometers during fast electromagnetic transients

Thread Summary

The user inquired about using the ADXL1005 accelerometer in a variable magnetic field (0 to 1 T in 1 s, stable for 1 s, then a fast transient of 0.1 T in 1 ms). The final answer indicates that the magnetic field should not affect the ADXL1005's operation, as the datasheet suggests magnetic mounting for low-frequency acceleration. No shielding is recommended for the accelerometer or cabling.
AI Generated Content

I was wondering if I could use ADXL1005 at a variable magnetic field (increase from 0 to 1 T in 1 s, then stable magnetic field for 1 s, then fast transient 0.1 T in 1 ms)? 

Would you recommend any shielding for the accelerometer and/or cabling?

Thank you

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.