Post Go back to editing

Question about NULL_CNFG for IMU device

Thread Summary

The user asked about the function of NULL_CNFG for IMU devices and its availability on the ADIS16480. The engineer clarified that the ADIS16480 uses the Tare command in the GLOB_CMD register for auto-nulling, which orients the IMU's axes to East/North/Up (ENU) and sets pitch and roll to 0 degrees. The NULL_CFG in Table 3 refers to the stall time required for the Tare command. Setting the Body Frame bit in the EKF_CONFIG register to 1 allows viewing accelerometer readings relative to the IMU's orientation.
AI Generated Content

I have some questions about NULL_CNFG(Continous bias estimation) for IMU devices.

#1, what's the function of NULL_CNFG? If you have some material to explain this function, please let me know.

#2, About ADIS16480, Table3 says mention “NULL_CNFG” stall times, but I can’t find “NULL_CNFG" on the register of USE REGISTERS map.
Is it possible to use NULL_CFG on ADIS16480?
(It looks like ADIS16489 has the NULL_CFG register on the user reg map)

https://www.analog.com/media/en/technical-documentation/data-sheets/ADIS16480.pdf

Best,

Tarzan2

Parents
  • Hello Tarzan2,

    I have a correction from what I previously wrote. The ADIS16480 has auto-nulling function, and it's in the GLOB_CMD register labeled as a Tare command. "NULL_CFG" in Table 3 of the datasheet is the amount of time required to complete this command. 

    The goal of this command is the orient the IMUs x/y/z axes to East/North/Up (ENU) by using the reference transformation matrix as described on Page 30 of the datasheet. After the tare function, assuming the local navigation frame is selected, the IMU will report 0 deg pitch, and 0 deg roll, and the accelerometers will read x=0g, y=0g, and z=1g, even though the IMU wasn't necessarily laying flat during execution of the Tare command. If you want to see what the accelerometers read relative to the orientation of the IMU, set the Body Frame bit in the EKF_CONFIG register to 1.

    I hope this helps, and I apologize for the confusion.

    -Paul Kern

  • Hi Paul, 

    I'm sorry that I could not replay quickly.

    I understand what you mean. Thanks for the answer.

    Best regards,

    Tarzan2

Reply Children
No Data